ping fail with switch ports on LSDK20.04 v5.4 kernel image and rootfs on nxp-ls1028

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ping fail with switch ports on LSDK20.04 v5.4 kernel image and rootfs on nxp-ls1028

831 Views
hittzt
Contributor V

Hi experts,

I am now working on testing the tsn functionality on felix switch of nxp-ls1028, and I find that

the ping fail with two boards(board A and board B) connected by swp0s with the switch configs as LSDK2004 user manual:

ifconfig eno2 up
ip link add name switch type bridge
ip link set switch up
ip link set swp0 master switch && ip link set swp0 up
ip link set swp1 master switch && ip link set swp1 up
ip link set swp2 master switch && ip link set swp2 up
ip link set swp3 master switch && ip link set swp3 up

Set switch ip on two board, and ping each other:

$ ifconfig switch 192.168.1.2 /* On board A */
$ ifconfig switch 192.168.1.3 /* On board B */
$ ping 192.168.1.3 /* On board A */

ping shows:

root@localhost:~/tsntest/linuxptp-configs# ping 192.168.1.3
PING 192.168.1.3 (192.168.1.3) 56(84) bytes of data.
From 192.168.1.2 icmp_seq=1 Destination Host Unreachable
From 192.168.1.2 icmp_seq=2 Destination Host Unreachable
From 192.168.1.2 icmp_seq=3 Destination Host Unreachable

and on board A, it did not get the mac of board B 

root@localhost:~/tsntest/linuxptp-configs# arp -a
? (192.168.1.1) at <incomplete> on switch
? (192.168.1.3) at <incomplete> on switch

on board B, it got the mac of board A successfully:

root@localhost:~/tsntest/linuxptp-configs# arp -a
? (192.168.1.2) at 6a:1f:1e:02:cc:69 [ether] on switch

the kernel version on these two boards is the same:

Linux localhost 5.4.3 #3 SMP PREEMPT Tue Jun 9 17:17:31 CST 2020 aarch64 aarch64 aarch64 GNU/Linux

Is there any known issues on switch ports?

Thanks,

Zhantao

0 Kudos
4 Replies

746 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the attached script and test log.

0 Kudos

746 Views
hittzt
Contributor V

Hi Yiping,

Thanks for your reply.

The script and log you give me are no bridge mode, 

is there any logs of bridge mode like my question and the LSDK20.04 user manual show?

Thanks,

Zhantao

0 Kudos

746 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the attachment.

0 Kudos

746 Views
hittzt
Contributor V

Hi Yiping,

Thanks for your reply.

I will check it.

Thanks,

Zhantao

0 Kudos