p2020 identified as p2010

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

p2020 identified as p2010

Jump to solution
592 Views
wangxiao
Contributor II

Hi,

   We using the chip P2020,but when read System version register(GUTS_SVR),the result is 

0x80EB 0021 for P2010。Why does this happen?

1 Solution
524 Views
r8070z
NXP Employee
NXP Employee


Have a great day,

Check that TEST_SEL pin is not pulled down. P2020 requires for pull up with a 4.7 k resistor to OVdd on this pin.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
525 Views
r8070z
NXP Employee
NXP Employee


Have a great day,

Check that TEST_SEL pin is not pulled down. P2020 requires for pull up with a 4.7 k resistor to OVdd on this pin.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------