p1022 bootup crash - DDR address space issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

p1022 bootup crash - DDR address space issue

524 Views
zeevg
Contributor I

Hi,

Our bootup of the p1022 is crash every time.

we recognize access to incorrect address location, not assigned to any memory target.

The bootup fail on address 0x20090000 which is inside the DDR MMU address space but out of the actual DDR size.

 

From the init file we running for the bootup I see the followed DDR address space definition:

 

  1. DDR global address space: 2G

 

                # LAWAR11

                # bit 0 = 1 - enable window

                # bit 7-11 = 01111 - DDR

                # bit 26 - 31 =  011110 2G - size

                mem [CCSR 0xd70] = 0x80f0001e

 

  1. DDR MMU address space: 1G

 

                # define 1GB      TLB1 entry 1: 0x00000000 - 0x3FFFFFFF; DDR, cacheable, not guarded

                reg ${CAM_GROUP}L2MMU_CAM1 = 0xA0007FC41C0800000000000000000001

 

  1. DDR size: 512M

 

                #CS0_BNDS

                mem [CCSR 0x2000] = 0x0000001F

                #CS0_CNFG

                mem [CCSR 0x2080] = 0x80014202

 

 

could you see problems with the ddr address space definition?

Do I need to change the DDR MMU address space to 512 M ?

could you have advise how to proceed?

Zeev Gerber

0 Kudos
3 Replies

407 Views
Bulat
NXP Employee
NXP Employee

Your settings are incorrect of course, even in the DDR controller:.

--------------------------------------------------------------

                #CS0_BNDS

                mem [CCSR 0x2000] = 0x0000001F

this corresponds to 512MB memory size.

---------------------------------------------------------------

                #CS0_CNFG

                mem [CCSR 0x2080] = 0x80014202

This corresponds to 1GB memory size assuming 64-bit DDR bus.

---------------------------------------------------------------

So it is unclear what is correct memory size in your case, but you need to set all LAWAR, MMU and DDR controller to the same value.

Regards,

Bulat

0 Kudos

407 Views
zeevg
Contributor I

Hi,

    # DDR_SDRAM_CFG
    mem [CCSR 0x2110] = 0x470c0008

we are working with 32-bit DDR bus, so we have 512MB memory size.

When we configure the CS0 to 256MB memory size the bootup stop crash.

we are working now on half of our ddr memory space.

Are the DRAM controller support 512MB memory size when working with 32-bit DDR bus?

Pls. advise

0 Kudos

406 Views
Bulat
NXP Employee
NXP Employee

Ok, so 512MB is correct memory size. Yes, it is supported with 32-bit DDR bus. Now you need to set  DDR's LAWAR and MMU to the same size.

0 Kudos