mpc8309 pci endpoint configure

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

mpc8309 pci endpoint configure

758 次查看
威杨
Contributor III

I  use mpc8309 as pci ep device under uboot, i configure  pci_ctrl->pitar0 = 0x7F00000,pci_ctrl->pibar0 = 0x80000000,pci_ctrl->piwar0 = 0x80055013, when pci root device write and read correspond endpoint ddr 0 address, not 0x7f00000,i need your help. 

THANKS.

标签 (1)
0 项奖励
回复
1 回复

592 次查看
Pavel
NXP Employee
NXP Employee

Check the PCI Local Access Window Register (PCILAWBAR0) and PCI Local Access Window Attributes Register (PCILAWAR) settings. See attached files.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复