memac10 independent mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

memac10 independent mode

402件の閲覧回数
MarkPalamar
Contributor I

Is it possible to run memac10 in independent mode on the t2081 processor?  A board is configuring memac10 to use the second RGMII interface.  Memac3 is using the first RGMII interface and works fine in independent mode.  However memac10 is 1 / 2.5 / 10Gbps, so I'm wondering if it can not be used in independent mode.

Thanks!

Mark

0 件の賞賛
1 返信

367件の閲覧回数
ufedor
NXP Employee
NXP Employee

The T2081 mEMAC10 can operate in independent mode.

0 件の賞賛