ls1046a nand flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ls1046a nand flash

2,664件の閲覧回数
hongyuanz
Contributor IV

Hi ,

We are using LS1046A Based custom board. We are booting PBL and U-boot from QSPI Flash and we want to boot dpl, dpc, dtb, kernel and filesystem from NAND flash.

What to do with nand flash ..?

Thanks.

0 件の賞賛
返信
4 返答(返信)

2,650件の閲覧回数
Pavel
NXP Employee
NXP Employee

See the Section 4.3.7 in LSDK 2108 User Guide about .itb file building and loading:

https://www.nxp.com/docs/en/user-guide/LSDKUG_Rev21.08.pdf

0 件の賞賛
返信

2,662件の閲覧回数
hongyuanz
Contributor IV

1 U-boot from QSPI Flash
2 kernel and filesystem from NAND flash
Is there any corresponding documentation ..?

0 件の賞賛
返信

2,193件の閲覧回数
kairovr
Contributor I
Hi,

Did you managed to boot the U-boot from QSPI Flash and then boot the kernel and filesystem from NAND flash? Or did you found any documentation on how to do this?

BR.
0 件の賞賛
返信

2,185件の閲覧回数
hongyuanz
Contributor IV

hi kairovr

Yes, you can help. . ?

0 件の賞賛
返信