ls1046a nand flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ls1046a nand flash

2,672 Views
hongyuanz
Contributor IV

Hi ,

We are using LS1046A Based custom board. We are booting PBL and U-boot from QSPI Flash and we want to boot dpl, dpc, dtb, kernel and filesystem from NAND flash.

What to do with nand flash ..?

Thanks.

0 Kudos
Reply
4 Replies

2,658 Views
Pavel
NXP Employee
NXP Employee

See the Section 4.3.7 in LSDK 2108 User Guide about .itb file building and loading:

https://www.nxp.com/docs/en/user-guide/LSDKUG_Rev21.08.pdf

0 Kudos
Reply

2,670 Views
hongyuanz
Contributor IV

1 U-boot from QSPI Flash
2 kernel and filesystem from NAND flash
Is there any corresponding documentation ..?

0 Kudos
Reply

2,201 Views
kairovr
Contributor I
Hi,

Did you managed to boot the U-boot from QSPI Flash and then boot the kernel and filesystem from NAND flash? Or did you found any documentation on how to do this?

BR.
0 Kudos
Reply

2,193 Views
hongyuanz
Contributor IV

hi kairovr

Yes, you can help. . ?

0 Kudos
Reply