ls1043 sd boot,no log output

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ls1043 sd boot,no log output

2,022件の閲覧回数
412149526
Contributor I

We customized the ls1043 board and boot from the sd card. Now plug in the sd card, but there is no output from the serial port, we have checked and the voltage and power-on sequence are normal, can there be other places to check

タグ(1)
0 件の賞賛
返信
5 返答(返信)

1,978件の閲覧回数
ufedor
NXP Employee
NXP Employee

Use a digital scope and check:

1) RCW is read from the SD card

2) RESET_REQ_B is not asserted after the RCW readout

0 件の賞賛
返信

1,978件の閲覧回数
412149526
Contributor I

Whether the serder configuration is incorrect will also cause problems with startup

0 件の賞賛
返信

1,978件の閲覧回数
ufedor
NXP Employee
NXP Employee

Incorrect SerDes configuration will initiate RESET_REQ_B assertion.

0 件の賞賛
返信

1,978件の閲覧回数
412149526
Contributor I

How to check that the SerDes configuration is correct, which aspects need to be checked? Thank you!

0 件の賞賛
返信

1,978件の閲覧回数
ufedor
NXP Employee
NXP Employee

It is needed to refer to the QorIQ LS1043A Reference Manual, Table 33-1. Supported SerDes options and Table 33-4. Valid SerDes RCW Encodings and Reference Clocks.

0 件の賞賛
返信