I want to know the amplitude range and the rise time for the 48MHz clock input of the LS1024
48Mhz clock input (PS_XI) is a crystal input, it requires 3.3V sinusoidal input. Therefore, no slew rate is specified.
Have a great day,
Alexander,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------