ls1021a unable to disable SERDES module with RCW

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ls1021a unable to disable SERDES module with RCW

Jump to solution
1,634 Views
marcojankovic
Contributor II

hi everyone,

i m facing problemes with a microcontroler based on ls1021a (it is the tqmls1021a-cc). We are trying to disable the SERDES module with the RCW using the  ref manual. section  32.1.1.1.2.1 procedure.

PBL preamble and RCW header                                                                                                                            

aa55aa55 01ee0100

 0             32              64            92                                                                                                                            

 0608000a 00000000 00000000 00000000

128          160           192            224

FF000000 00C07900 40025a00 21046000 (boot failures)

07000000 00007900 40025a00 21046000 ( with this configuration we boot. With any other one we don't)

256         288           320           352

00000000 00000000 00000000 000bc800

384         416           448           480         512

20124900 0004b340 00000000 00000000

Are we missing something in the procedure to disable the serdes module properly ?

We would like to  use etsec2 has RGMII. But we think that the SERDES module initialize some register during power on reset to force the controller to be in SGMII. this is why we need to be able to turn the SERDES module off.

We are basing our hypotesis on this from the refenrence manual :

20.5.8 Ethernet control register (eTSECx_ECNTRL)
ECNTRL is a register writable by the user to configure and initialize the eTSEC. Note
that the FIFM, GMIIM, TBIM, RMM, and RPM fields are read-only, having been set
after sampling signals at power-on-reset

and also on the SERDES protocole documentation.

So far we don't know yet if its possbile to configure etsec2 properly for RGMII mode with the SERDES module powered on.

We are using QCVS to generate RCW.

thank you for your support.

1 Solution
1,126 Views
ufedor
NXP Employee
NXP Employee

1) I could check RCW if it will be provided as binary image.

2) To configure the eTSEC2 into RGMII mode it is required to select RCW[EC2]=000 (RGMII2).

View solution in original post

0 Kudos
7 Replies
1,126 Views
marcojankovic
Contributor II

Hi Ufedor,

We found our problem, it was related to our pbi. For a while i was investigating only on the RCW side. At some point i went to check the pbi and a mistake was made.  There was a PBI command  (09ea00e4 10000000) that was writing to the SERDES modules and explained the undifined behavior we encountered about RGMII for etsec2.

Thank you for your support.

1,126 Views
ketingxin
Contributor II

I found the same problem about RCW,when writed “FF”or“C”in the RCW control word to disable the SerDes module, ls1020A boot failure.

 FF000000 00C07900 40025a00 21046000 (boot failures).

0 Kudos
1,126 Views
ufedor
NXP Employee
NXP Employee

Please create new thread if you did not implement the mentioned PBI command.

0 Kudos
1,126 Views
ufedor
NXP Employee
NXP Employee

Thank you for the update.

1,126 Views
ketingxin
Contributor II

pastedImage_2.png

SerDes PLL1 and PLL2 connect to GND,the ls1020 boot failure.

or

set the RCW control word like this,1020 boot failure too.

#PBL preamble and RCW header
aa55aa55 01ee0100

#enable IFC, disable QSPI and DSPI
0608000c 00000000 00000000 00000000
FF000000 08C08028 60040a00 81046000
00000000 00000000 00000000 0002a800
80000100 0004b548 00000000 00000000

0 Kudos
1,127 Views
ufedor
NXP Employee
NXP Employee

1) I could check RCW if it will be provided as binary image.

2) To configure the eTSEC2 into RGMII mode it is required to select RCW[EC2]=000 (RGMII2).

0 Kudos
1,126 Views
marcojankovic
Contributor II

Hi ufedor,

thanks for your reply,

The yellow field correspond to etsec 1,2 and 3 configurations (they are already set to 000 wich is RGMII).

The green one concerns the SERDES fields.

this is our current RCW wich we can boot on properly :

 0             32              64            92                                                                                                                            

 0608000a 00000000 00000000 00000000

128          160           192            224

70000000 00007900 40025a00 21046000

256         288           320           352

00000000 00000000 00000000 000bc800

384         416           448           480         512

20124900 0004b340 00000000 00000000

If the byte 128 value is 0x70, our module boots. But any try to change the SERDES mode leads to  boot failures.

We are using QCVS to build our RCW.

I attached to my reply our RCW binary generated with QCVS corresponding to our configuration that boots. (RCW_PBL.bin)

And our test with our RCW with the  SERDES  module off that does not boot based on the steps described in the ls1021a ref manual (32.1.1.1.2.1 Disabling unused SerDes modules) . To enable the generation of this RCW under QVCS, we had to unable the option "Enabling Ignore Constraints and non-Critical Errors option" (RCW_SERDES_OFF.bin)

thank you for your support.

Regards.

0 Kudos