is it possible to run an e5500 vm via kvm on a e6500 core?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

is it possible to run an e5500 vm via kvm on a e6500 core?

1,654 次查看
danmerrill
Contributor I

we have a qemu vm based on an e5500 core, and wanted to use kvm to speed up the virutalization. We are wondering if it possible to do this on an e6500 core or will it only be possible on an e5500 core? Thanks.

0 项奖励
回复
2 回复数

1,398 次查看
bpe
NXP Employee
NXP Employee

 Your question is answered in the SDK online documentation, check the link below:


 https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK/GUID-F42130CF-FA76-4941-AE02-C...


Have a great day,

Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,398 次查看
danmerrill
Contributor I

So from the link it sounds like the answer is no. In order to run an e5500 vcpu I would need to be on an e5500 core, in order to run an e6500 vm I would have to be on an e6500. Is that correct? Thanks.

0 项奖励
回复