is it possible to run an e5500 vm via kvm on a e6500 core?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

is it possible to run an e5500 vm via kvm on a e6500 core?

1,601件の閲覧回数
danmerrill
Contributor I

we have a qemu vm based on an e5500 core, and wanted to use kvm to speed up the virutalization. We are wondering if it possible to do this on an e6500 core or will it only be possible on an e5500 core? Thanks.

0 件の賞賛
返信
2 返答(返信)

1,345件の閲覧回数
bpe
NXP Employee
NXP Employee

 Your question is answered in the SDK online documentation, check the link below:


 https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK/GUID-F42130CF-FA76-4941-AE02-C...


Have a great day,

Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,345件の閲覧回数
danmerrill
Contributor I

So from the link it sounds like the answer is no. In order to run an e5500 vcpu I would need to be on an e5500 core, in order to run an e6500 vm I would have to be on an e6500. Is that correct? Thanks.

0 件の賞賛
返信