how to build linux kernel for P1011

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to build linux kernel for P1011

2,608 Views
alikobari
Contributor I

 

Hello,

 

 

I am trying to create a kernel for P1011 base board. I started by using an existing functional kernel configuration file .config. All component and memory are identical in this 2 board, just different processor. So I was hoping the kernel would work fine, but it did not and I am getting this error, after boot up:

 

I would appreciate any help in this matter,

 

 

U-Boot 2010.12-svn10008 (Nov 10 2014 - 17:38:13) ge4404

 

 

CPU:   P1011, Version: 1.1, (0x80e50011)

 

Core:  E500, Version: 5.1, (0x80212051)

 

Clock Configuration:

 

       CPU0:800  MHz,

 

       CCB:400  MHz,

 

       DDR:333.333 MHz (666.667 MT/s data rate) (Asynchronous), LBC:25   MHz

 

L1:    D-cache 32 kB enabled

 

       I-cache 32 kB enabled

 

I2C:   ready

 

SPI:   ready

 

DRAM:  Configuring DDR for 666.667 MT/s data rate

 

DDR: 2 GiB (DDR3, 32-bit, CL=6, ECC off)

 

FLASH: 128 MiB

 

L2:    256 KB enabled

 

NAND:  1024 MiB

 

MMC:  FSL_ESDHC: 0

 

EEPROM: Read failed.

 

PCIe1: Root Complex of Slot 2, x2, regs @ 0xffe0a000

 

  01:00.0     - 14e4:b240 - Network controller

 

PCIe1: Bus 00 - 01

 

PCIe2: disabled

 

In:    serial

 

Out:   serial

 

Err:   serial

 

Net:   eTSEC3 is in sgmii mode.

 

eTSEC1: No support for PHY id 0; assuming generic

 

eTSEC2: No support for PHY id 0; assuming generic

 

eTSEC3: No support for PHY id 0; assuming generic

 

eTSEC1, eTSEC2, eTSEC3

 

bootmode 2: Booting RFS 1, Kernel 0

 

Hit any key to stop autoboot:  0

 

 

. done

 

Erased 1 sectors

 

  1. 9....8....7....6....5....4....3....2....1....WARNING: adjusting available memory to 30000000

 

## Booting kernel from Legacy Image at e8800000 ...

 

   Image Name:   Linux-3.0.34-ts-powerpc-rt55+

 

   Created:      2015-01-14  18:42:52 UTC

 

   Image Type:   PowerPC Linux Kernel Image (gzip compressed)

 

   Data Size:    3306175 Bytes = 3.2 MiB

 

   Load Address: 00000000

 

   Entry Point:  00000000

 

   Verifying Checksum ... OK

 

## Flattened Device Tree blob at e8080000

 

   Booting using the fdt blob at 0xe8080000

 

   Uncompressing Kernel Image ... OK

 

   Loading Device Tree to 00ffa000, end 00fff503 ... OK

 

WARNING: could not find compatiblenode fsl-usb2-dr: FDT_ERR_NOTFOUND.

 

WARNING: could not find compatible node fsl-usb2-dr: FDT_ERR_NOTFOUND.

 

Using P2020 RDB machine description

 

Memory CAM mapping: 256/256/256 Mb, residual: 1280Mb

 

Linux version 3.0.34-ts-powerpc-rt55+ (akobari@ubuntu) (gcc version 4.6.3 (Timesys 20130114) ) #5 SMP Wed Jan 14 13:42:47 EST 2015

 

CPU maps initialized for 1 thread per core

 

bootconsole [udbg0] enabled

 

setup_arch: bootmem

 

mpc85xx_rdb_setup_arch()

 

Found FSL PCI host bridge at 0x00000000ffe0a000. Firmware bus number: 0->1

 

PCI host bridge /pcie@ffe0a000  ranges:

 

MEM 0x0000000080000000..0x000000009fffffff -> 0x0000000080000000

 

  IO 0x00000000ffc00000..0x00000000ffc0ffff -> 0x0000000000000000

 

/pcie@ffe0a000: PCICSRBAR @ 0xfff00000

 

MPC85xx RDB board from Freescale Semiconductor

 

arch: exit

 

Zone PFN ranges:

 

  DMA      0x00000000 -> 0x00030000

 

  Normal   empty

 

  HighMem  0x00030000 -> 0x00080000

 

Movable zone start PFN for each node

 

early_node_map[1] active PFN ranges

 

    0: 0x00000000 -> 0x00080000

 

MMU: Allocated 1088 bytes of context maps for 255 contexts

 

PERCPU: Embedded 7 pages/cpu @c2009000 s4448 r8192 d16032 u32768

 

Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 520192

 

Kernel command line: console=ttyS0,115200 rootfstype=ubifs rw root=ubi0:rootfs ubi.mtd=7

 

PID hash table entries: 4096 (order: 2, 16384 bytes)

 

Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)

 

Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)

 

Memory: 2072916k/2097152k available (6340k kernel code, 24236k reserved, 280k data, 278k bss, 216k init)

 

Kernel virtual memory layout:

 

  * 0xfffbf000..0xfffff000  : fixmap

 

  * 0xff800000..0xffc00000  : highmem PTEs

 

  * 0xff7ec000..0xff800000  : early ioremap

 

  * 0xf1000000..0xff7ec000  : vmalloc & ioremap

 

SLUB: Genslabs=15, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1

 

Hierarchical RCU implementation.

 

NR_IRQS:512

 

mpic: Setting up MPIC " OpenPIC  " version 1.2 at ffe40000, max 1 CPUs

 

mpic: ISU size: 256, shift: 8, mask: ff

 

mpic: Initializing for 256 sources

 

clocksource: timebase mult[5000000] shift[22] registered

 

Console: colour dummy device 80x25

 

pid_max: default: 32768 minimum: 301

 

Mount-cache hash table entries: 512

 

Brought up 1 CPUs

 

devtmpfs: initialized

 

NET: Registered protocol family 16

 

            

 

PCI: Probing PCI hardware

 

pci 0000:00:00.0: ignoring class b20 (doesn't match header type 01)

 

pci 0000:00:00.0: PCI bridge to [bus 01-ff]

 

pci 0000:00:00.0: PCI bridge to [bus 01-01]

 

pci 0000:00:00.0: bridge window [io 0xff7ed000-0xff7fcfff]

 

pci 0000:00:00.0: bridge window [mem 0x80000000-0x9fffffff]

 

pci 0000:00:00.0: bridge window [mem pref disabled]

 

pci 0000:00:00.0: enabling device (0106 -> 0107)

 

bio: create slab <bio-0> at 0

 

raid6: int32x1    123 MB/s

 

raid6: int32x2    199 MB/s

 

raid6: int32x4    296 MB/s

 

raid6: int32x8    254 MB/s

 

raid6: using algorithm int32x4 (296 MB/s)

 

Freescale Elo / Elo Plus DMA driver

 

vgaarb: loaded

 

SCSI subsystem initialized

 

usbcore: registered new interface driver usbfs

 

usbcore: registered new interface driver hub

 

usbcore: registered new device driver usb

 

Switching to clocksource timebase

 

Switched to NOHz mode on CPU #0

 

NET: Registered protocol family 2

 

IP route cache hash table entries: 32768 (order: 5, 131072 bytes)

 

TCP established hash table entries: 131072 (order: 8, 1048576 bytes)

 

TCP bind hash table entries: 65536 (order: 7, 524288 bytes)

 

TCP: Hash tables configured (established 131072 bind 65536)

 

TCP reno registered

 

UDP hash table entries: 512 (order: 2, 16384 bytes)

 

UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)

 

NET: Registered protocol family 1

 

RPC: Registered named UNIX socket transport module.

 

RPC: Registered udp transport module.

 

RPC: Registered tcp transport module.

 

RPC: Registered tcp NFSv4.1 backchannel transport module.

 

fsl-elo-dma ffe0c300.dma: #0 (fsl,eloplus-dma-channel), irq 76

 

fsl-elo-dma ffe0c300.dma: #1 (fsl,eloplus-dma-channel), irq 77

 

fsl-elo-dma ffe0c300.dma: #2 (fsl,eloplus-dma-channel), irq 78

 

fsl-elo-dma ffe0c300.dma: #3 (fsl,eloplus-dma-channel), irq 79

 

fsl-l2ctlr ffe20000.l2-cache-controller: Entire L2 as cache, provide valid sram address and size

 

fsl-l2ctlr: probe of ffe20000.l2-cache-controller failed with error -22

 

fsl-elo-dma ffe21300.dma: #0 (fsl,eloplus-dma-channel), irq 21

 

fsl-elo-dma ffe21300.dma: #1 (fsl,eloplus-dma-channel), irq 22

 

fsl-elo-dma ffe21300.dma: #2 (fsl,eloplus-dma-channel), irq 23

 

fsl-elo-dma ffe21300.dma: #3 (fsl,eloplus-dma-channel), irq 24

 

fsl-pq_mdio: probe of ffe24520.mdio failed with error -16

 

audit: initializing netlink socket (disabled)

 

type=2000 audit(0.508:1): initialized

 

highmem bounce pool size: 64 pages

 

NTFS driver 2.1.30 [Flags: R/W].

 

JFFS2 version 2.2. (NAND) (SUMMARY)  © 2001-2006 Red Hat, Inc.

 

msgmni has been set to 1488

 

Block layer SCSI generic (bsg) driver version 0.4 loaded (major 254)

 

io scheduler noop registered

 

io scheduler deadline registered

 

io scheduler cfq registered (default)

 

Serial: 8250/16550 driver, 2 ports, IRQ sharing enabled

 

serial8250.0: ttyS0 at MMIO 0xffe04500 (irq = 42) is a 16550A

 

console [ttyS0] enabled, bootconsole disabled

 

console [ttyS0] enabled, bootconsole disabled

 

serial8250.0: ttyS1 at MMIO 0xffe04600 (irq = 42) is a 16550A

 

Generic non-volatile memory driver v1.1

 

brd: module loaded

 

loop: module loaded

 

e8000000.nor: Found 1 x16 devices at 0x0 in 16-bit bank. Manufacturer ID 0x000001 Chip ID 0x002801

 

Amd/Fujitsu Extended Query Table at 0x0040

 

  Amd/Fujitsu Extended Query version 1.5.

 

number of CFI chips: 1

 

Creating 6 MTD partitions on "e8000000.nor":

 

0x000000000000-0x000000080000 : "NOR,512KB, Boot Configuration"

 

0x000000080000-0x000000100000 : "NOR,512KB, DTB Image"

 

0x000000100000-0x000000800000 : "NOR, 7MB Reserved"

 

0x000000800000-0x000001000000 : "NOR,8MB Linux Kernel 0"

 

0x000001000000-0x000001800000 : "NOR,8MB Linux Kernel 1"

 

0x000007f80000-0x000008000000 : "NOR,512KB, U-BOOT Boot Loader"

 

NAND device: Manufacturer ID: 0x01, Chip ID: 0xd3 (AMD NAND 1GiB 3,3V 8-bit)

 

Creating 3 MTD partitions on "ffa00000.flash":

 

0x000000000000-0x00001f000000 : "NAND,496MB UBIFS 0"

 

0x00001f000000-0x00003e000000 : "NAND,496MB UBIFS 1"

 

0x00003e000000-0x000040000000 : "32MB for Fastpath Configuration"

 

eLBC NAND device at 0xffa00000, bank 1

 

UBI: attaching mtd7 to ubi0

 

UBI: physical eraseblock size:   131072 bytes (128 KiB)

 

UBI: logical eraseblock size:    129024 bytes

 

UBI: smallest flash I/O unit:    2048

 

UBI: sub-page size:              512

 

UBI: VID header offset:          512 (aligned 512)

 

UBI: data offset:                2048

 

UBI: max. sequence number:       47

 

UBI: attached mtd7 to ubi0

 

UBI: MTD device name:            "NAND,496MB UBIFS 1"

 

UBI: MTD device size:            496 MiB

 

UBI: number of good PEBs:        3968

 

UBI: number of bad PEBs:         0

 

UBI: number of corrupted PEBs:   0

 

UBI: max. allowed volumes:       128

 

UBI: wear-leveling threshold:    4096

 

UBI: number of internal volumes: 1

 

UBI: number of user volumes:     1

 

UBI: available PEBs:             0

 

UBI: total number of reserved PEBs: 3968

 

UBI: number of PEBs reserved for bad PEB handling: 39

 

UBI: max/mean erase counter: 1/0

 

UBI: image sequence number: 1750748030

 

UBI: background thread "ubi_bgt0d" started, PID 1039

 

INFO: rcu_sched_state detected stall on CPU 0 (t=15000 jiffies)

 

INFO: rcu_sched_state detected stall on CPU 0 (t=60030 jiffies)

 

INFO: rcu_sched_state detected stall on CPU 0 (t=105060 jiffies)

 

INFO: rcu_sched_state detected stall on CPU 0 (t=150090 jiffies)

 

INFO: rcu_sched_state detected stall on CPU 0 (t=195120 jiffies)

 

INFO: rcu_sched_state detected stall on CPU 0 (t=240150 jiffies)

 

INFO: rcu_sched_state detected stall on CPU 0 (t=285180 jiffies)

 

INFO: rcu_sched_state detected stall on CPU 0 (t=330210 jiffies)

 

INFO: rcu_sched_state detected stall on CPU 0 (t=375240 jiffies)

 

INFO: rcu_sched_state detected stall on CPU 0 (t=420270 jiffies)

 

INFO: rcu_sched_state detected stall on CPU 0 (t=465300 jiffies)

 

INFO: rcu_sched_state detected stall on CPU 0 (t=510330 jiffies)

 

INFO: rcu_sched_state detected stall on CPU 0 (t=555360 jiffies)

 

INFO: rcu_sched_state detected stall on CPU 0 (t=600390 jiffies)

 

INFO: rcu_sched_state detected stall on CPU 0 (t=645420 jiffies)

 

INFO: rcu_sched_state detected stall on CPU 0 (t=690450 jiffies)

 

INFO: rcu_sched_state detected stall on CPU 0 (t=735480 jiffies)

 

INFO: rcu_sched_state detected stall on CPU 0 (t=780510 jiffies)

 

INFO: rcu_sched_state detected stall on CPU 0 (t=825540 jiffies)

 

INFO: rcu_sched_state detected stall on CPU 0 (t=870570 jiffies)

 

INFO: rcu_sched_state detected stall on CPU 0 (t=915600 jiffies)

 

INFO: rcu_sched_state detected stall on CPU 0 (t=960630 jiffies)

 

INFO: rcu_sched_state detected stall on CPU 0 (t=1005660 jiffies)

 

INFO: rcu_sched_state detected stall on CPU 0 (t=1050690 jiffies)

 

INFO: rcu_sched_state detected stall on CPU 0 (t=1095720 jiffies)

 

INFO: rcu_sched_state detected stall on CPU 0 (t=1140750 jiffies)

 

INFO: rcu_sched_state detected stall on CPU 0 (t=1185780 jiffies)

 

INFO: rcu_sched_state detected stall on CPU 0 (t=1230810 jiffies)

 

INFO: rcu_sched_state detected stall on CPU 0 (t=1275840 jiffies)

 

INFO: rcu_sched_state detected stall on CPU 0 (t=1320870 jiffies)

 

INFO: rcu_sched_state detected stall on CPU 0 (t=1365900 jiffies)

 

INFO: rcu_sched_state detected stall on CPU 0 (t=1410930 jiffies)

 

INFO: rcu_sched_state detected stall on CPU 0 (t=1455960

 

0 Kudos
Reply
3 Replies

2,075 Views
scottwood
NXP Employee
NXP Employee

Why are you using such an old kernel?  I suggest trying the latest upstream kernel (or if you prefer, the latest Freescale SDK kernel).  Or, if you really want to run this TimeSys kernel, you should seek support from TimeSys.

What was the "different processor" that you had been using?

BTW, it's hard to read logs that have a blank line between each line...

0 Kudos
Reply

2,075 Views
alikobari
Contributor I

Hello Scott,

Thanks for reply, I have no choice except to use this kernel:: Linux version 3.0.34-ts-powerpc-rt55+ (akobari@ubuntu) (gcc version 4.6.3 (Timesys 20130114)  which is part of a broader product component we use in my company, and I thought Linux version 3.0 is pretty up-to-date,. Any way that's not the issue because I am using the exact kernel for our other board,  based on P2020 processor with no issue at all. I am also in contact with TimeSys community as well. I just want to get as much as help I can get to solve my problem.   The log file I attached was captured by my editor, and I did  not realized it has extra line in between!!!


Again I am using the same kernel by TimeSys with the same .config for P2020 based board, so there is an identical uImage for both and one is working fine the other stuck in this INFO message:


INFO: rcu_sched_state detected stall on CPU

INFO: rcu_sched_state detected stall on CPU

INFO: rcu_sched_state detected stall on CPU


it looks like the cpu is waiting for some events


Ali,

0 Kudos
Reply

2,075 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Ali Kobari,

A customer reported a similar problem previously, please check whether it would be helpful to use "nohz=off" Kernel boot parameter to disable dyntick-idle mode.

An idle CPU that is not receiving scheduling-clock interrupts is said to be "dyntick-idle". The CONFIG_NO_HZ_IDLE=y Kconfig option causes the kernel to avoid sending scheduling-clock interrupts to idle CPUs, which is critically important both to battery-powered devices and to highly virtualized mainframes.

Therefore, system with aggressive real-time response constraints often run CONFIG_HZ_PERIODIC=y kernels(or CONFIG_NO_HZ=n) in order to avoid degrading from-idle transition latencies.

This boot parameter "nohz=" that can be used to disable dyntick-idle mode in CONFIG_NO_HZ_IDLE=y kernel by specifying "nohz=off". By the default, the system boot with "nohz=on", enabling dyntick-idle mode.



Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply