evalboard for LS1043 and CPLD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

evalboard for LS1043 and CPLD

1,043件の閲覧回数
trondwang
Contributor I

Hi NXP!

we have bought the evalboard for LS1043. This board has a CPLD. We have downloaded the source code for the CPLD, but it would be helpful if we had the testbench for the code. Can you provide us with the testbench?

regards Trond Wang

#ls1043a‌, CPLD

タグ(1)
0 件の賞賛
5 返答(返信)

796件の閲覧回数
trondwang
Contributor I

Hi pro-supportengineer

LS1043ARDB-PA_CPLD_V1.4.zip does not contain a testbench as far as I can see.

0 件の賞賛

796件の閲覧回数
pro-supportengi
NXP Employee
NXP Employee

Does the LS1043ARDB-PA_CPLD_V1.4.zip also contain a CPLD testbench?

0 件の賞賛

796件の閲覧回数
trondwang
Contributor I

Hi NXP,

the reason for asking for the testbench file is to better understand the functions of the verilog code programmed into the CPLD. The designer of the evaluation board presumably have this file.

regards Trond Wang

0 件の賞賛

796件の閲覧回数
ufedor
NXP Employee
NXP Employee

The "LS1043A-RDB Rev B Design Files" package contains complete CPLD project (LS1043ARDB-PA_CPLD_V1.4.zip).

0 件の賞賛

796件の閲覧回数
ufedor
NXP Employee
NXP Employee

Why you need the testbench?

Shouldn't it be requested from the CPLD manufacturer?

0 件の賞賛