effective RAM size on P2041

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

effective RAM size on P2041

1,750 Views
emintz
Contributor I

Hi everybody,

I use P2041RDB. My RTOS kernel (loaded as elf image) occupies only 120 MB of the RAM memory. How can I configure u-boot

to initialize and use only 256MB instead of available 2GB on the board.

Thanks,

Eli

0 Kudos
Reply
3 Replies

1,599 Views
r8070z
NXP Employee
NXP Employee


Have a great day,

It is not clear what is "effective RAM size". I think u-boot should initiate all 2GB even in case when it is possible to init only 256 MB from 2GB physically. It is not possible on the P2041RDB with single 2GB SODIMM.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,599 Views
emintz
Contributor I

Hi Serguei,

You mean if I change RAM size in the configuration file P2041RDB.h, any changes would happen ?

Eli

0 Kudos
Reply

1,599 Views
lunminliang
NXP Employee
NXP Employee

Hello Eli Mintz,

I think you would like to change the memory mapping and the MMU setting in board\freescale\p1_p2_rdb_pc\Law.c and board\freescale\p1_p2_rdb_pc\Tlb.c.

Regards

Lunmin

0 Kudos
Reply