Hi everybody,
I use P2041RDB. My RTOS kernel (loaded as elf image) occupies only 120 MB of the RAM memory. How can I configure u-boot
to initialize and use only 256MB instead of available 2GB on the board.
Thanks,
Eli
Have a great day,
It is not clear what is "effective RAM size". I think u-boot should initiate all 2GB even in case when it is possible to init only 256 MB from 2GB physically. It is not possible on the P2041RDB with single 2GB SODIMM.
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Eli Mintz,
I think you would like to change the memory mapping and the MMU setting in board\freescale\p1_p2_rdb_pc\Law.c and board\freescale\p1_p2_rdb_pc\Tlb.c.
Regards
Lunmin