does T4240 can use two srio port as the same time?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

does T4240 can use two srio port as the same time?

899 次查看
xinjiezhang
Contributor I

if the 2 srio port can use same times,the ID is same?@

0 项奖励
回复
1 回复

819 次查看
ufedor
NXP Employee
NXP Employee

Yes, the T4240 supports SerDes configuration when two SRIO controllers are used simultaneously.

0 项奖励
回复