Hello,
i want to make some timing tests and dont want to have any jitter due to dualthreading. Is it possible to disable it and if, how?
Best regards and thanks for your answers in advance
Please look e6500 Core Reference Manual, Section 2.15.1.2 "Thread Enable (TEN) Register".
This register shows which threads are enabled. By default the only one thread 0 is enabled.
TEN is read-only register, enabling and disabling should be done via TENS and TENC registers.
Direct link to e6500 Core Reference Manual:
https://www.nxp.com/docs/en/reference-manual/E6500RM.pdf
Have a great day,
Alexander,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------