configuration inputs in t2081

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

configuration inputs in t2081

1,429件の閲覧回数
monalihaware
Contributor III

i ahve a custom board using t2081. with hard coded rcw sysclk=133mhz and ddrclk=66mhz..

followed the connections as per the RDB. But at reset, the configuration inputs which should be pulled '1' automatically  by the processor are '0'. Has any one encountered this problem? N what could be the solution? any help please

タグ(2)
0 件の賞賛
返信
1 返信

1,388件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please refer to the processor's Data Sheet and doublecheck that following points are considered/fulfilled:

1) note 5 after the Table 1. Pinout list by bus

2) 3.2 Power sequencing

3) 3.5 Power-on ramp rate

0 件の賞賛
返信