configuration inputs in t2081

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

configuration inputs in t2081

1,388 次查看
monalihaware
Contributor III

i ahve a custom board using t2081. with hard coded rcw sysclk=133mhz and ddrclk=66mhz..

followed the connections as per the RDB. But at reset, the configuration inputs which should be pulled '1' automatically  by the processor are '0'. Has any one encountered this problem? N what could be the solution? any help please

标记 (2)
0 项奖励
回复
1 回复

1,347 次查看
ufedor
NXP Employee
NXP Employee

Please refer to the processor's Data Sheet and doublecheck that following points are considered/fulfilled:

1) note 5 after the Table 1. Pinout list by bus

2) 3.2 Power sequencing

3) 3.5 Power-on ramp rate

0 项奖励
回复