building the layerscape sdk: Source repos unreachable

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

building the layerscape sdk: Source repos unreachable

2,083 Views
hardsoft
Contributor II

I am building this from with the docker environment, which has functioning DNS and web access:

root@fbubuntu:~# flex-builder -m ls1012ardb -a arm64
MACHINE: ls1012ardb
DESTARCH: arm64
INSTRUCTION: autobuild
MACHINE: ls1012ardb

CONFIGLIST: build_lsdk_internal.cfg
make: Entering directory '/home/qoriq/flexbuild/packages/firmware'

fetch firmware repositories ...

repo: dash-uboot
branch = devel
Cloning into 'dash-uboot'...
fatal: repository 'https://bitbucket.sw.nxp.com/scm/dash/dash-uboot/' not found

repo: dash-rcw
branch = devel
Cloning into 'dash-rcw'...
fatal: repository 'https://bitbucket.sw.nxp.com/scm/dash/dash-rcw/' not found

repo: qoriq-uefi-binary
branch = master
Cloning into 'qoriq-uefi-binary'...
fatal: repository 'https://bitbucket.sw.nxp.com/scm/dash/qoriq-uefi-binary/' not found

repo: qoriq-fm-ucode
branch = sdk-v2.0.x
Cloning into 'qoriq-fm-ucode'...
fatal: repository 'https://bitbucket.sw.nxp.com/scm/dpaamodules/fm-ucode/' not found

repo: mc-utils
branch = master
Cloning into 'mc-utils'...
fatal: repository 'https://bitbucket.sw.nxp.com/scm/dash/mc-utils/' not found

repo: qoriq-mc-binary
branch = lsdk
Cloning into 'qoriq-mc-binary'...
fatal: repository 'https://bitbucket.sw.nxp.com/scm/dpaa2/mc-binary/' not found

repo: ppa-generic
branch = master
Cloning into 'ppa-generic'...
fatal: repository 'https://bitbucket.sw.nxp.com/scm/dnnpi/ppa-generic/' not found

repo: qoriq-qe-ucode
branch = master
Cloning into 'qoriq-qe-ucode'...
fatal: repository 'https://bitbucket.sw.nxp.com/scm/dash/qoriq-qe-ucode/' not found

repo: qoriq-firmware-cortina
branch = master
Cloning into 'qoriq-firmware-cortina'...
fatal: repository 'https://bitbucket.sw.nxp.com/scm/dash/qoriq-firmware-cortina/' not found

repo: qoriq-engine-pfe-bin
branch = master
Cloning into 'qoriq-engine-pfe-bin'...
fatal: repository 'https://bitbucket.sw.nxp.com/scm/dncpe/engine-pfe-bin/' not found
Makefile:288: recipe for target 'repo_fetch' failed
make: *** [repo_fetch] Error 128
make: Leaving directory '/home/qoriq/flexbuild/packages/firmware'

5 Replies

1,418 Views
danlenz
Contributor II

Same here 18.09 - how could a bug this serious that was known in 18.06 not be fixed in 18.09? Is there a work around? 18.09 appears to be unusable otherwise.

1,418 Views
georgehubbard
Contributor II

I am getting the same issue with LSDK 1809

1,418 Views
vijay1
Contributor II

Same here. Also, there are no prior versions of flex-builder available for download - at least I am not seeing it.

0 Kudos

1,418 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello hardsoft,

It seems that previously an internal testing version LSDK 1806 package was uploaded to the git hub by mistake, those links mentioned above are for internal use.

Please download LSDK 1806 again from Layerscape SDK|NXP, the correct formal released version has been uploaded now.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

1,418 Views
vijay1
Contributor II

Hello Yiping,

Is there any update on this? LSDK 1806 is not downloadable. The link you provided takes us to version 1809 and I am not seeing any references to 1806. As pointed out in this thread and in another, version 1809 is a non-starter. I can't even go beyond even the basic steps as all references are pointing to your internal git repositories. I am unable to comprehend how this got released for general audience.

Can we at the least get a response as to when we can expect a fix?

Thanks and regards,

0 Kudos