boot method of ARDB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

boot method of ARDB

Jump to solution
1,196 Views
junfeng_zhang
Contributor I

Dear NXP(ARDB) expert:

Thank you very much. 

BR/Junfeng

0 Kudos
1 Solution
838 Views
ufedor
NXP Employee
NXP Employee

Please refer to the following Community question:

https://community.nxp.com/message/1079924 

View solution in original post

0 Kudos
5 Replies
838 Views
ufedor
NXP Employee
NXP Employee
0 Kudos
838 Views
junfeng_zhang
Contributor I

Thank you Ufedor:)

BR/Junfeng

0 Kudos
838 Views
ufedor
NXP Employee
NXP Employee

There is no pre-built SD boot image for the LS2088ARDB.

Please use a debugger and restore NOR or QSPI firmware image available at:

LSDK Open Source 

LSDK IMAGES

0 Kudos
839 Views
ufedor
NXP Employee
NXP Employee

Please refer to the following Community question:

https://community.nxp.com/message/1079924 

0 Kudos
838 Views
ufedor
NXP Employee
NXP Employee

On the LS2085ARDB/LS2088ARDB revisions D – F, switch SW9 bits 3:5 control which bank the SoC loads from when it powers up.

When SW9[3:5] = OFF-OFF-OFF - NOR Flash Bank 0 is selected. With this settings the NOR Flash bank 0 is started from address 0x580000000.

0 Kudos