Yocto for the b4860qds-64b

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Yocto for the b4860qds-64b

698 Views
midnight
Contributor I

Can I get support for using Yocto to build an image for the b4860qds-64b?

Thanks,

K

0 Kudos
Reply
2 Replies

606 Views
bpe
NXP Employee
NXP Employee

Yes, you can build a Linux image for B4860 PowerPC core with QorIQ SDK. Download the SDK source and cache images and follow the install/prepare/build instructions:

https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK/GUID-E19DF47A-0188-4032-8975-B...

Deployment instructions for your board can be found here:

https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK/GUID-29B421EF-3638-47E7-A6B6-9...


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

606 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Kyle Unice,

I have moved this thread to the QorIQ community space so it gets addressed.

Rgeards,

0 Kudos
Reply