Why does the LS1012AFRWY Rev C board not support SD card boot?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why does the LS1012AFRWY Rev C board not support SD card boot?

Jump to solution
1,196 Views
pholden
Contributor III

I am using flex-builder to build custom kernel driver and user app for a client's system based on the LS1XXX.  I got an LS1012AFRWY REVC to do some preliminary work prior to receiving prototype hardware.  The board has an onboard microSD, so I assumed I can boot via microSD as I've done for many boards.  Here is what happens when I run flex-builder:

 

flex-builder -c firmware -m ls1012afrwy -b sd

.

.

.

make[2]: Leaving directory '/media/Projects/iSpace/LS10xx/newyocto/flexbuild_lsdk2108_github/components/firmware/atf'
ls1012afrwy sdboot is not supported

 

Is there a work-around for this?

Thanks!

 

0 Kudos
Reply
1 Solution
1,100 Views
Oswalag
NXP TechSupport
NXP TechSupport

Yes, it is possible.

Please refer to chapter 4.1.5.4 Automatically download and deploy LSDK images of the LSDK2108UG.

Regards.

View solution in original post

6 Replies
1,170 Views
pholden
Contributor III

Thanks for the quick response.   That's most unfortunate.  Is there documentation or procedure on how to program the qspi from a linux host PC?

 

Thanks.

0 Kudos
Reply
1,127 Views
Oswalag
NXP TechSupport
NXP TechSupport

Hello,

 

The procedure is available in chapter 3.7.1.3 Program Layerscape LDP composite firmware image (In the LLDPUG)
To program the Layerscape LDP composite firmware image in the QSPI NOR flash on FRWY-LS1012A:

0 Kudos
Reply
1,184 Views
Oswalag
NXP TechSupport
NXP TechSupport

Hello,

Unfortunately the LS1012A is the only one from the Layerscape devices that doesn't support booting from SD card, only from QuadSPI. 

Regards.

0 Kudos
Reply
1,166 Views
pholden
Contributor III

Can flex-installer be used to program the qspi for LS1012AFRWY?

0 Kudos
Reply
1,101 Views
Oswalag
NXP TechSupport
NXP TechSupport

Yes, it is possible.

Please refer to chapter 4.1.5.4 Automatically download and deploy LSDK images of the LSDK2108UG.

Regards.

1,109 Views
pholden
Contributor III

How about TFTPBOOT?  Is there a document/user-guide on how to boot via TFTP for LS1012A-FRWY using flex-builder images?

0 Kudos
Reply