Why does the LS1012AFRWY Rev C board not support SD card boot?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Why does the LS1012AFRWY Rev C board not support SD card boot?

跳至解决方案
1,262 次查看
pholden
Contributor III

I am using flex-builder to build custom kernel driver and user app for a client's system based on the LS1XXX.  I got an LS1012AFRWY REVC to do some preliminary work prior to receiving prototype hardware.  The board has an onboard microSD, so I assumed I can boot via microSD as I've done for many boards.  Here is what happens when I run flex-builder:

 

flex-builder -c firmware -m ls1012afrwy -b sd

.

.

.

make[2]: Leaving directory '/media/Projects/iSpace/LS10xx/newyocto/flexbuild_lsdk2108_github/components/firmware/atf'
ls1012afrwy sdboot is not supported

 

Is there a work-around for this?

Thanks!

 

0 项奖励
回复
1 解答
1,166 次查看
Oswalag
NXP TechSupport
NXP TechSupport

Yes, it is possible.

Please refer to chapter 4.1.5.4 Automatically download and deploy LSDK images of the LSDK2108UG.

Regards.

在原帖中查看解决方案

6 回复数
1,236 次查看
pholden
Contributor III

Thanks for the quick response.   That's most unfortunate.  Is there documentation or procedure on how to program the qspi from a linux host PC?

 

Thanks.

0 项奖励
回复
1,193 次查看
Oswalag
NXP TechSupport
NXP TechSupport

Hello,

 

The procedure is available in chapter 3.7.1.3 Program Layerscape LDP composite firmware image (In the LLDPUG)
To program the Layerscape LDP composite firmware image in the QSPI NOR flash on FRWY-LS1012A:

0 项奖励
回复
1,250 次查看
Oswalag
NXP TechSupport
NXP TechSupport

Hello,

Unfortunately the LS1012A is the only one from the Layerscape devices that doesn't support booting from SD card, only from QuadSPI. 

Regards.

0 项奖励
回复
1,232 次查看
pholden
Contributor III

Can flex-installer be used to program the qspi for LS1012AFRWY?

0 项奖励
回复
1,167 次查看
Oswalag
NXP TechSupport
NXP TechSupport

Yes, it is possible.

Please refer to chapter 4.1.5.4 Automatically download and deploy LSDK images of the LSDK2108UG.

Regards.

1,175 次查看
pholden
Contributor III

How about TFTPBOOT?  Is there a document/user-guide on how to boot via TFTP for LS1012A-FRWY using flex-builder images?

0 项奖励
回复