Why does the LS1012AFRWY Rev C board not support SD card boot?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Why does the LS1012AFRWY Rev C board not support SD card boot?

ソリューションへジャンプ
1,304件の閲覧回数
pholden
Contributor III

I am using flex-builder to build custom kernel driver and user app for a client's system based on the LS1XXX.  I got an LS1012AFRWY REVC to do some preliminary work prior to receiving prototype hardware.  The board has an onboard microSD, so I assumed I can boot via microSD as I've done for many boards.  Here is what happens when I run flex-builder:

 

flex-builder -c firmware -m ls1012afrwy -b sd

.

.

.

make[2]: Leaving directory '/media/Projects/iSpace/LS10xx/newyocto/flexbuild_lsdk2108_github/components/firmware/atf'
ls1012afrwy sdboot is not supported

 

Is there a work-around for this?

Thanks!

 

0 件の賞賛
返信
1 解決策
1,208件の閲覧回数
Oswalag
NXP TechSupport
NXP TechSupport

Yes, it is possible.

Please refer to chapter 4.1.5.4 Automatically download and deploy LSDK images of the LSDK2108UG.

Regards.

元の投稿で解決策を見る

6 返答(返信)
1,278件の閲覧回数
pholden
Contributor III

Thanks for the quick response.   That's most unfortunate.  Is there documentation or procedure on how to program the qspi from a linux host PC?

 

Thanks.

0 件の賞賛
返信
1,235件の閲覧回数
Oswalag
NXP TechSupport
NXP TechSupport

Hello,

 

The procedure is available in chapter 3.7.1.3 Program Layerscape LDP composite firmware image (In the LLDPUG)
To program the Layerscape LDP composite firmware image in the QSPI NOR flash on FRWY-LS1012A:

0 件の賞賛
返信
1,292件の閲覧回数
Oswalag
NXP TechSupport
NXP TechSupport

Hello,

Unfortunately the LS1012A is the only one from the Layerscape devices that doesn't support booting from SD card, only from QuadSPI. 

Regards.

0 件の賞賛
返信
1,274件の閲覧回数
pholden
Contributor III

Can flex-installer be used to program the qspi for LS1012AFRWY?

0 件の賞賛
返信
1,209件の閲覧回数
Oswalag
NXP TechSupport
NXP TechSupport

Yes, it is possible.

Please refer to chapter 4.1.5.4 Automatically download and deploy LSDK images of the LSDK2108UG.

Regards.

1,217件の閲覧回数
pholden
Contributor III

How about TFTPBOOT?  Is there a document/user-guide on how to boot via TFTP for LS1012A-FRWY using flex-builder images?

0 件の賞賛
返信