Why does NAND flash have only 0x1300000(20MB or so) address mapping on ls1043a-rdb board?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why does NAND flash have only 0x1300000(20MB or so) address mapping on ls1043a-rdb board?

528 Views
zumengchen
Contributor III

Hi experts,

My board ls1043a-rdb with REV B1 serial number: TR15260008

According to the board schematic and the kernel driver as follows:

nand: device found, Manufacturer ID: 0x2c, Chip ID:0xac

nand: Micron MT29F4G08ABBDAH4

nand: 512MiB, SLC, page size: 2048, OOB size: 64

So I think MT29F4G08ABBDAH4 has been equipped within the board, and I noticed

there is a address mapping in dts definition of arch/arm64/boot/dts/freescale/fsl-ls1043a-rdb.dts

    /* NOR, NAND Flashes and FPGA on board */
    ranges = <0x0 0x0 0x0 0x60000000 0x08000000
              0x1 0x0 0x0 0x7e800000 0x00010000
              0x2 0x0 0x0 0x7fb00000 0x00000100>;

But it seems there is only 0x1300000(20MB or so), I wonder if this has a relationship with FPGA?

or this NAND is used to be memory for FPGA?

How culd Linux kernel use all 512MB ?

Cheers,

Zumeng

0 Kudos
1 Reply

428 Views
zumengchen
Contributor III

Ignored this issue please, I'm wrong on this issue, thanks

0 Kudos