Where are the SmartDSP Network demos for B4860 ? We want to do TCP and UDP comms to an SC3900 DSP Core.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where are the SmartDSP Network demos for B4860 ? We want to do TCP and UDP comms to an SC3900 DSP Core.

736 Views
billchadwick
Contributor III

I can't see any Ethernet / IP networking stuff in C:\Freescale\CW_SC_v10.8.0\SC\StarCore_Support\SmartDSP

We have some IP networking applications on 8156 / SC3850 and are wanting to port to B4860 / SC3900

Tags (2)
0 Kudos
4 Replies

521 Views
catalindemergia
Contributor IV

Hi,

SmartDSP had a networking stack when the SC was standalone, but in B4860 there are also

PA cores that run Linux. You will not find networking demos for SC.

regards,

Catalin

0 Kudos

521 Views
billchadwick
Contributor III

Catalin,

To confirm.

Its not just the demos that are missing, rather, there is no IP stack support in SmartDSP for SC3900 - despite it being mentioned in the Code Warrior 10.8 Smart DSP OS User Guide at section 1.2.4

Bill

0 Kudos

521 Views
catalindemergia
Contributor IV

Hi,

It could be that this information is old (before the architecture changes)

and the user guide needs to be updated.

I will check with the team.

Catalin

0 Kudos

521 Views
catalindemergia
Contributor IV

Hi,

I logged a bug to the documentation team to update the document.

regards,

Catalin

0 Kudos