I can't see any Ethernet / IP networking stuff in C:\Freescale\CW_SC_v10.8.0\SC\StarCore_Support\SmartDSP
We have some IP networking applications on 8156 / SC3850 and are wanting to port to B4860 / SC3900
Hi,
SmartDSP had a networking stack when the SC was standalone, but in B4860 there are also
PA cores that run Linux. You will not find networking demos for SC.
regards,
Catalin
Catalin,
To confirm.
Its not just the demos that are missing, rather, there is no IP stack support in SmartDSP for SC3900 - despite it being mentioned in the Code Warrior 10.8 Smart DSP OS User Guide at section 1.2.4
Bill
Hi,
It could be that this information is old (before the architecture changes)
and the user guide needs to be updated.
I will check with the team.
Catalin
Hi,
I logged a bug to the documentation team to update the document.
regards,
Catalin