When will the : LS1043ARDB-PA eval board as well as the associated BSP be available?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

When will the : LS1043ARDB-PA eval board as well as the associated BSP be available?

Jump to solution
1,295 Views
donberkowitz
Contributor II

Question is the same as the title line...

0 Kudos
Reply
1 Solution
1,147 Views
bpe
NXP Employee
NXP Employee

LS1043RDB-PA is a valid, active part number:

QorIQ LS1043A-RDB|NXP

Contact a distributor in your region for local availability.

SDK 0.4 is available for download:

QorIQ LS1043A and LS1023A Multicore Communica|NXP


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,148 Views
bpe
NXP Employee
NXP Employee

LS1043RDB-PA is a valid, active part number:

QorIQ LS1043A-RDB|NXP

Contact a distributor in your region for local availability.

SDK 0.4 is available for download:

QorIQ LS1043A and LS1023A Multicore Communica|NXP


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply