When P4080/T2080 secure boot , use wrong key to sign the u-boot ,the u-boot can boot up normally.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

When P4080/T2080 secure boot , use wrong key to sign the u-boot ,the u-boot can boot up normally.

1,082 Views
liyan
Contributor I

I'm working on secure boot for T2080QDS.I find an issue ,when we use wrong key to sign the u-boot ,the u-boot still can boot up.

Below is my steps ,

Brun Key1 to flash ,

Use other key Key2 to sign the u-boot ,

Burn u-boot and header into flash ,reboot the device ,the u-boot can boot up.

  We do the same test in P4080 board ,it has same issue

U-Boot 2016.012.0+ga9b437f (Jul 14 2016 - 15:55:35 +0800)

Environment size: 1729/8188 bytes

=> tftp 1000000 secure_boot/p4080/hdr_uboot.out

Using FM1@DTSEC1 device

TFTP from server 128.224.167.34; our IP address is 128.224.162.23

Filename 'secure_boot/p4080/hdr_uboot.out'.

Load address: 0x1000000

Loading: *

TFTP error: 'File not found' (1)

Not retrying...

=> tftp 1000000 secure_boot/p4080/hdr_uboot.out.t2080_key

Using FM1@DTSEC1 device

TFTP from server 128.224.167.34; our IP address is 128.224.162.23

Filename 'secure_boot/p4080/hdr_uboot.out.t2080_key'.

Load address: 0x1000000

Loading: #

done

Bytes transferred = 1280 (500 hex)

=> erase ecb00000 +500

. done

Erased 1 sectors

=> cp.b 1000000 ecb00000 500

Copy to Flash... 9....8....7....6....5....4....3....2....1....done

=>

U-Boot 2016.012.0+ga9b437f (Jul 13 2016 - 19:59:54 +0800)

CPU0:  P4080E, Version: 2.0, (0x82080020)

Core:  e500mc, Version: 2.0, (0x80230020)

Clock Configuration:

       CPU0:1499.985 MHz, CPU1:1499.985 MHz, CPU2:1499.985 MHz, CPU3:1499.985 MHz,

       CPU4:1499.985 MHz, CPU5:1499.985 MHz, CPU6:1499.985 MHz, CPU7:1499.985 MHz,

       CCB:799.992 MHz,

       DDR:649.994 MHz (1299.987 MT/s data rate) (Asynchronous), LBC:99.999 MHz

       FMAN1: 599.994 MHz

       FMAN2: 599.994 MHz

       QMAN:  399.996 MHz

       PME: 599.994 MHz

L1:    D-cache 32 KiB enabled

       I-cache 32 KiB enabled

Reset Configuration Word (RCW):

       00000000: 105a0000 00000000 1e1e181e 0000cccc

       00000010: 40464003 3c3c2000 dea00000 e1000000

       00000020: 00000000 00000000 00000000 008b6000

       00000030: 00000000 00000000 00000000 00000000

I2C:   ready

Board: P4080DS, Sys ID: 0x17, Sys Ver: 0x01, FPGA Ver: 0x0a, vBank: 0

SERDES Reference Clocks: Bank1=100MHz Bank2=125MHz Bank3=125MHz

SPI:   ready

DRAM:  Initializing....using SPD

Detected UDIMM HMT125U7BFR8C-H9

Detected UDIMM HMT125U7BFR8C-H9

2 GiB left unmapped

Testing 0x00000000 - 0x7fffffff

Testing 0x80000000 - 0xffffffff

Remap DDR 2 GiB left unmapped

4 GiB (DDR3, 64-bit, CL=9, ECC on)

       DDR Controller Interleaving Mode: cache line

       DDR Chip-Select Interleaving Mode: CS0+CS1

POST memory PASSED

Flash: 128 MiB

L2:    128 KiB enabled

Corenet Platform Cache: 2 MiB enabled

SRIO1: disabled

SRIO2: disabled

MMC:   FSL_SDHC: 0

Using default environment

EEPROM: Invalid ID (ff ff ff ff)

PCIe1: Root Complex, no link, regs @ 0xfe200000

PCIe1: Bus 00 - 00

PCIe2: disabled

PCIe3: Root Complex, no link, regs @ 0xfe202000

PCIe3: Bus 01 - 01

In:    serial

Out:   serial

Err:   serial

Net:   Fman1: Uploading microcode version 106.2.9

Fman2: Uploading microcode version 106.2.9

Could not get PHY for P4080DS_MDIO8: addr 28

Failed to connect

Could not get PHY for P4080DS_MDIO8: addr 29

Failed to connect

Could not get PHY for P4080DS_MDIO1: addr 0

Failed to connect

FM1@DTSEC2

Error: FM1@DTSEC2 address not set.

, FM2@DTSEC1

Error: FM2@DTSEC1 address not set.

, FM2@DTSEC2

Error: FM2@DTSEC2 address not set.

, FM2@TGEC1

Error: FM2@TGEC1 address not set.

Hit any key to stop autoboot: 0

esbc_validate command successful

## Executing script at e8a00000

esbc_validate command successful

esbc_validate command successful

WARNING: adjusting available memory to 30000000

## Booting kernel from Legacy Image at e8020000 ...

   Image Name:   vxworks

   Image Type:   PowerPC VxWorks Kernel Image (uncompressed)

   Data Size:    1862808 Bytes = 1.8 MiB

   Load Address: 00100000

   Entry Point:  00100000

   Verifying Checksum ... OK

## Flattened Device Tree blob at e8800000

   Booting using the fdt blob at 0xe8800000

   Loading Kernel Image ... OK

   Loading Device Tree to 03fe9000, end 03fff03d ... OK

## Starting vxWorks at 0x00100000, device tree at 0x03fe9000 ...

Hello, VxWorks!

0 Kudos
3 Replies

851 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Li Yan,

The behavior you see is correct, the system wouldn’t reset if there is mismatch in the hash, and would continue when we do secure boot with SB_EN=1.

The system would get reset for this error , if you secure boot with ITS=1. (blowing fuse ITS)

To stop system from moving further / reset with SB_EN=1, try removing the header of the bootscript from flash. You will get a barker code error and system will reset.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

851 Views
liyan
Contributor I

Hi Yiping,

   If we set the ITS to board , it cannot be change. And if we want boot this board ,we must sign the image , am I right?

0 Kudos

851 Views
yipingwang
NXP TechSupport
NXP TechSupport

Yes, you are right. After blowing fuse ITS, the board only can be used for secure boot.

Thanks,

Yiping

0 Kudos