What is the purpose of using '1588 TEST HEADER' in LS1046A-RDB?

cancel
Showing results for 
Search instead for 
Did you mean: 

What is the purpose of using '1588 TEST HEADER' in LS1046A-RDB?

370 Views
sun_lee
Contributor I

Hi, I have a question in the schematics of LS1046A-RDB.

I don't know what the purpose of using '1588 TEST HEADER' in LS1046A-RDB.

So, i want to know what the purpose of using '1588 TEST HEADER' and how to use it.

Thanks.

0 Kudos
1 Reply

275 Views
alexander_yakov
NXP Employee
NXP Employee

The IEEE 1588 block has several input and output pins - PULSE_OUT, ALARM_OUT, TRIG_IN. These pins are routed out to IEEE 1588 test header to have a possibility to illustrate IEEE 1588 functionality. For example you can connect two boards together via Ethernet with IEEE 1588 synchronization enabled, and than connect dual-beam scope to pulse outputs of each IEEE 1588 test headers and see, how they run synchronously, when Ethernet cable is connected, and loose synchronization when disconnected.


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos