What is the maximum memory supported by T4240 and T2080

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the maximum memory supported by T4240 and T2080

2,146 Views
siderealNight
Contributor I

The T4240 has 1 TB address space. Does that mean you can support up to 3 TB RAM?

 

What is the the maximum value for T2080?

 

thank you

0 Kudos
Reply
3 Replies

2,125 Views
siderealNight
Contributor I

Hi, thanks

" Chip Select is 16 pieces, that is 16 x 8Gb = 16GBytes. "

Should that not be 128 GB? , leading to 3 * 4* 128 = 1536 GB ?

Sorry for the trivial question, thank you.

0 Kudos
Reply

2,123 Views
Bulat
NXP Employee
NXP Employee

Gb means Gbit, i.e. 8Gb = 1GByte. So calculations are correct.

 

0 Kudos
Reply

2,132 Views
Bulat
NXP Employee
NXP Employee

There are some restrictions of course. When you ask "...can support up to 3 TB RAM?", you probably mean RAM like DDR? Here the T4240 is not a bottleneck, problem is rather with the RAM itself.

The T4240 supports DDR3/L memory and contains three DDR controllers with four memory banks (Chip Selects) each. In turn the the maximum volume of DDR3L devices is 8Gb. Assuming the user uses x4 devices and 64-bit bus width, the number of devices per one Chip Select is 16 pieces, that is 16 x 8Gb = 16GBytes. For Chip Selects provide 4 x 16GBytes = 64GBytes. So three DDR controllers can support maximum 3 x 64GByes = 192Gbytes, that is maximum supported DDR size.

The T2080 supports only x8 and x16 device organization, so in maximum it supports 8 x 8Gb =8GBytes per one CS and 4 x 8Gbytes = 32Gbytes per the DDR controller, i.e. per the T2080.

These numbers can be found in the Ref Manuals, see sections 'Supported DDR SDRAM Organizations' .

Regards,

Bulat

 

0 Kudos
Reply