What is the difference between T2080RDB and T4240RDB on new software ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the difference between T2080RDB and T4240RDB on new software ?

459 Views
omer_er
Contributor I

Hello,

I downloaded latest kernel with yocto for T2080 and T4240 RDBs. I have run a few tests with SDK2.0 kernel and yocto kernel (which has a version 5.4.3). 

The results for T4240RDB are better with higher version kernel which comes with yocto; but results for T2080RDB are worse with higher version kernel.

I use traffic provider to generate 66Byte fixed packets at 10Gbps line rate. I used  2*10G ports on same RDB to forward traffic to each other. The tests are same for a single T2080RDB and T4240RDB.

The results are:

66Byte %100 line rate 10Gbps traffic to each port:

T2080RDB SDK 2.0 RX rate                 ~2.290Gbps

T2080RDB yocto 5.4.3 kernel RX rate  ~1.680Gbps

T4240RDB SDK 2.0 RX rate                 ~3.390 Gbps

T4240RDB yocto 5.4.3 kernel RX rate  ~4.590 Gbps

 

Why newer version of kernel worse than older version for T2080RDB ?

T4240RDB's performance is better for newer version.

 

What is the difference between T2080RDB and T4240RDB on new software ?

 

Any help will be appreciated

Thanks

0 Kudos
1 Reply

421 Views
yipingwang
NXP TechSupport
NXP TechSupport

Did you do L2 or L3 forwarding? Can you please describe your setup/configuration and the command that you ran on T2080 host?

0 Kudos