What is the clock rate between P2010 DDR controller and SDRAM part?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What is the clock rate between P2010 DDR controller and SDRAM part?

1,450 次查看
xiao-dong_wang
Contributor I

I have a P2010NSE2HHC processor. For the DDR controller, when DDRCLK input is 66.7 Hz and cfg_ddr_pll[0:2] is set to 0b100 (10:1 ratio), is the DDR controller running at 667MHz and the clock between the DDR controller and the SDRAM part running at 333MHz?

Thank you

0 项奖励
回复
3 回复数

1,384 次查看
xiao-dong_wang
Contributor I

For the P2010NSE2HHC, would the maximum for the DDR controller clock be 800MHz and so the clock between the DDR controller and the SDRAM part would max out at 400MHz?

Thank you

0 项奖励
回复

1,384 次查看
Bulat
NXP Employee
NXP Employee

Yes, MCK frequency would be 400MHz and data rate - 800MT/s.

Regards,

Bulat

0 项奖励
回复

1,384 次查看
Bulat
NXP Employee
NXP Employee

Yes, that is correct.

Regards,

Bulat

0 项奖励
回复