What is specific CPU Frequency of the processor on P2020RDB: P2020 Reference Design Board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What is specific CPU Frequency of the processor on P2020RDB: P2020 Reference Design Board

797 次查看
sagee
Contributor I

I'm considering purchasing the P2020RDB but I can not seem to find any information on which P2020 is being used.  I need to find the CPU speed of the processor used.

0 项奖励
回复
1 回复

719 次查看
r8070z
NXP Employee
NXP Employee


Have a great day,

Typically the P2020RDB has P2020 QorIQ 1200MHZ 1.05V TEPBGA689. The P2020RDB-PCA Quick Start Guide says:

“Key Features of the P2020RDB-PCA 

  Freescale QorIQ architecture CPU

   QorIQ P2020E, 1200 MHz "

I expect that P2020NSE2MHC is installed on the currently available P2020RDB-PCA board. However you may ask the board distributor for confirmation.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复