What drives USBx_DRVVBUS pin high or low?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What drives USBx_DRVVBUS pin high or low?

1,278 Views
will_alarcon
Contributor I

Hi, I am trying to use the USB on the LS1020A as a host and have a quick question regarding the DRVVBUS pin. What drives this pin high or low?

Thank you,

Will Alarcon

Tags (3)
0 Kudos
1 Reply

1,165 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Will Alarcon,

Please refer to "AN4878, QorIQ LS1021A Design Checklist" which could be downloaded from QorIQ® Layerscape 1020A | NXP .

USBx_DRVVBUS VBUS power enable.Optional. For example, if an external hub is used, it can handle this signal.

The functionalityVBUS signal is determined by the RCW[SDHC] field in the reset configuration word.

USB2_DRVVBUS The functionality of this signal is determined by the EC1 field in the reset configuration word (RCW[EC3]).

Thanks,

Yiping

0 Kudos