I'm trying to determine the meaning of the suffix in NXP part numbers such as T1040D4RDB-PA.
At the time I write this question, it appears that T1040D4RDB-PA is available on the NXP site. I'm trying to determine what the difference is between this and T1040RDB-PC. Thanks to a post on this site, I understand that the D4 refers to DDR4 memory. What is the meaning of the "-PA" or "-PC" suffix? Is it a version specifier?
The WindRiver site shows BSP support for T1040RDB-PC. If this suffix is a version specifier, then WindRiver seems to indicate support for a version after the one that I can obtain from NXP.
Any input would be appreciated.
Solved! Go to Solution.
Yes, suffix "-PA" or "-PC" at the end of partnumber indicates board revision. Note T1040RDB and T1040D4RDB are two different boards, with different revision numbering, and T1040D4RDB-PA is more recent than T1040RDB-PC
Yes, the main difference between non-D4 and D4 boards is in DDR4 memory used.
Have a great day,
Alexander
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Yes, suffix "-PA" or "-PC" at the end of partnumber indicates board revision. Note T1040RDB and T1040D4RDB are two different boards, with different revision numbering, and T1040D4RDB-PA is more recent than T1040RDB-PC
Yes, the main difference between non-D4 and D4 boards is in DDR4 memory used.
Have a great day,
Alexander
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------