We are using LS1043A, in that we are using both EC1 and EC2.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

We are using LS1043A, in that we are using both EC1 and EC2.

跳至解决方案
701 次查看
logeshs
Contributor II

Both EC1 and EC2 are connected as RGMII. We have connected EC1 to one PHY and EC2 to Switch. Can we use either EMI1/EMI2 alone (single management Interface) for both EC1 and EC2?

Suppose if we use both Management interface EMI1 and EMI2, shall we connect any of the management interface EMI to either of EC1 or EC2? is there any restriction that EC1 should be connected with EMI1 & EC2 with EMI2? 

0 项奖励
1 解答
561 次查看
bpe
NXP Employee
NXP Employee

Any PHY in the system can be connected to any externally visible
management interface, regardless of the data path connection.
EMI1 and EMI2, however, are not identical. Their pin drivers are
fed from different power supplies and only EMI2 supports IEEE802.3 Clause 45
extensions. See LS1043A Datasheet, Section 3.11.6 for details.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
2 回复数
561 次查看
logeshs
Contributor II

Thanks for your clarification

0 项奖励
562 次查看
bpe
NXP Employee
NXP Employee

Any PHY in the system can be connected to any externally visible
management interface, regardless of the data path connection.
EMI1 and EMI2, however, are not identical. Their pin drivers are
fed from different power supplies and only EMI2 supports IEEE802.3 Clause 45
extensions. See LS1043A Datasheet, Section 3.11.6 for details.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励