We are using LS1043A, in that we are using both EC1 and EC2.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

We are using LS1043A, in that we are using both EC1 and EC2.

ソリューションへジャンプ
1,499件の閲覧回数
logeshs
Contributor II

Both EC1 and EC2 are connected as RGMII. We have connected EC1 to one PHY and EC2 to Switch. Can we use either EMI1/EMI2 alone (single management Interface) for both EC1 and EC2?

Suppose if we use both Management interface EMI1 and EMI2, shall we connect any of the management interface EMI to either of EC1 or EC2? is there any restriction that EC1 should be connected with EMI1 & EC2 with EMI2? 

0 件の賞賛
返信
1 解決策
1,359件の閲覧回数
bpe
NXP Employee
NXP Employee

Any PHY in the system can be connected to any externally visible
management interface, regardless of the data path connection.
EMI1 and EMI2, however, are not identical. Their pin drivers are
fed from different power supplies and only EMI2 supports IEEE802.3 Clause 45
extensions. See LS1043A Datasheet, Section 3.11.6 for details.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,359件の閲覧回数
logeshs
Contributor II

Thanks for your clarification

0 件の賞賛
返信
1,360件の閲覧回数
bpe
NXP Employee
NXP Employee

Any PHY in the system can be connected to any externally visible
management interface, regardless of the data path connection.
EMI1 and EMI2, however, are not identical. Their pin drivers are
fed from different power supplies and only EMI2 supports IEEE802.3 Clause 45
extensions. See LS1043A Datasheet, Section 3.11.6 for details.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信