We are using LS1043A, SPI chip select and GPIO muxed query

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

We are using LS1043A, SPI chip select and GPIO muxed query

1,097件の閲覧回数
logeshs
Contributor II

we are using 2 SPI devices with LS1043A, I need to use the remaining chipselects as GPIOs. could you help me what value should i keep in RCW of SPI_BASE[382-383] and SPI_EXT[360-362]?

0 件の賞賛
返信
2 返答(返信)

949件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

If my understanding is correct, I think this question is fully answered in Table 3-8 "SPI Signal configuration" of the LS1043A Reference Manual.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

949件の閲覧回数
logeshs
Contributor II

I understand i need to keep SPI_BASE[382-383] as 00, But i'm confused with what value should i keep on SPI_EXT[360-362]. Please suggest me the SPI_EXT[360-362] bit value such that i can use the remaining chip selects as GPIOs

0 件の賞賛
返信