Hello Serge,
T4240 Rev 2.0 fix some limitations of T4240 Rev 1.0.
For board boot up, the RCW and PBI commands are different, please pay attention to RCW field MEM_PLL_RAT.
MEM_PLL_RAT on T4240 Rev2.0 uses a value which is half of Rev1.0, it's 12 in Rev1.0, for Rev2.0 it uses 6.
Please make sure you have already flash Rev 2.0 RCW on the alternate bank.
I attached the Freescale u-boot patch for your reference.
If necessary you could create a service request to require AN4713 about the hardware difference between T4240 Rev1 and Rev2.
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------