Hi,
I would like to ask if VSPs and oNICs are supported on T2080rdb since I read somewhere in the manual, where only B4 and T4 platforms were supported.
Hello Heena S,
In theory, VSP(Virtual Storage Profiles) and oNICs are supported on T2080.
VSP is supported in DPAA FMAN 3.x architecture.
ONIC Ethernet Driver has fsl,dpa-ethernet-generic as compatible string in the device tree, there are only available use cases for T4 and B4 in Linux Kernel, you need to do the porting for yourself.
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello yipingwang,
Thanks, I managed to get it working.