Using Yocto/Pocky Linux SDK to build a specific kernel version?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Using Yocto/Pocky Linux SDK to build a specific kernel version?

4,194 次查看
jonbrogdon
Contributor I

I am relatively new to Yocto/Poky.  I have customized and built kernels and rootfs for various QorIQ targets (P1022DS, MPC8544DS, and MPC8572DS) using the Linux SDK Poky build system.  My question is: how would I go about building a specific version of the kernel for given target?  I need to build a 2.6 kernel for the MPC8572--specifically, 2.6.32-rc5.  When I build this kernel using Linux SDK 1.2, I get a 3.0 kernel.

I've considered 2 approaches for this:

#1.  Downloading the 2.6.32-rc5 kernel tarball to the sources directory in my build tree, and modifying the recipes to build this kernel.

#2.  Construct a build tree from Freescale git repositories.  At least then I could use "git checkout v2.6.32-rc5" tag for the linux repository.

Using either approach I get stuck on the fact that I don't know which recipes need modifying to build the kernel and rootfs.  Approach #1 seems like it should be easy.  But, I like approach #2 as I feel like I would learn more about the build system in general.

Any suggestions here are welcome.

4 回复数

2,807 次查看
timurtabi
Contributor III

Our QorIQ SDKs support only a single kernel version for all SOCs.  We call it a "unified kernel", and we do that intentionally.

If you need an older kernel version, then you probably need to look upstream and download the specific version you want.  You'll then need to identify all the missing features that you need, and manually back-port them.

2.6.32 is really old.  There's no support for the P1022 in that kernel.  Some support exists in 2.6.35, but most code was added after that.

2,807 次查看
scottwood
NXP Employee
NXP Employee

...and if you really, really need 2.6.32 for some reason, why a release candidate rather than the latest bugfix release 2.6.32.60?

0 项奖励
回复

2,807 次查看
jonbrogdon
Contributor I

We have existing products based on the 2.6.32-rc5 kernel--with several custom patches for our HW.  Eventually, we would move forward with a newer kernel.  I am trying to bring up a quick prototype.

0 项奖励
回复

2,807 次查看
scottwood
NXP Employee
NXP Employee

The difference between 2.6.32-rc5 and 2.6.32.60 should just be bugfixes with little to no impact on your custom patches.

0 项奖励
回复