Use P2010 in avionic system

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Use P2010 in avionic system

1,320件の閲覧回数
fernandoalcaide
Contributor II

Dear,

I´m seaching one processor to avionic system, P2010 is a good processor to my application but I need if this processor is use in avionic application?

Thank you in advance

0 件の賞賛
返信
1 返信

1,217件の閲覧回数
LPP
NXP Employee
NXP Employee

P2010/P2020 can be used for avionic application with the following remark.

Freescale doesn't qualify Power PC processors for Military or aerospace applications. If you need specificaly qualified products, ask our partners like e2v.

"The Hi-rel microprocessors are based on commercial products selected, qualified, screened and packaged to satisfy the most severe environmental conditions. e2v is supporting the PowerPC microprocessor in extended and military temperature and a range of critical peripherals such as PCI bridge, clock driver, and communication controllers. "

http://www.e2v.com/products/semiconductors/high-reliability-microprocessors/?resources#56


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信