Use IGH master stack to make my p1010rdb-pb board serve as an EtherCAT master

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Use IGH master stack to make my p1010rdb-pb board serve as an EtherCAT master

594 Views
tcguchengjie
Contributor II

Hello,I have a p1010rdb-pb board.I hear that yocto doesn't support EtherCAT master stack on this board.So I wonder if I can use  open source code,such as IGH,to make my board serve as an EtherCAT master.Anything related is welcome.Thanks in advance.

0 Kudos
1 Reply

407 Views
Pavel
NXP Employee
NXP Employee

Look at the following pages:

http://www.nxp.com/products/software-and-tools/hardware-development-tools/tower-development-boards/p...

and

http://www.nxp.com/products/microcontrollers-and-processors/power-architecture-processors/qoriq-powe...

See also the following:

http://cache.freescale.com/files/ftf_2010/Americas/WBNR_FTF10_IND_F0762.pdf?fsrch=1&sr=6&pageNum=1


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos