Hello,I have a p1010rdb-pb board.I hear that yocto doesn't support EtherCAT master stack on this board.So I wonder if I can use open source code,such as IGH,to make my board serve as an EtherCAT master.Anything related is welcome.Thanks in advance.
Look at the following pages:
and
See also the following:
http://cache.freescale.com/files/ftf_2010/Americas/WBNR_FTF10_IND_F0762.pdf?fsrch=1&sr=6&pageNum=1
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------