Unable to ping to u-boot in T2080RDB from Linux host PC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to ping to u-boot in T2080RDB from Linux host PC

ソリューションへジャンプ
2,337件の閲覧回数
singhawadhesh
Contributor I

Hi Team,

I have enabled the 1G RGMII (RTL8211E) ethernet ports (Port FM1@DTSEC3 in U-boot and port fm1-mac3 in linux) on the t2080 reference board, assigned IP address using dhcp. However, I am unable to ping to the t2080 board u-boot from the linux PC.

From U-boot if I try this connection (ping 10.60.101.107) I get a response. But since linux I configure the network but I do not get the answer.

In linux I follow the following steps to configure the network:

1) vi /etc/network/interfaces

2) I add the following lines in the interface file:

      auto fm1-mac3

      iface fm1-mac3 inet static

      address 10.60.101.109

      net mask 255.255.255.0

3) From the console I execute:

      ifup  -a fm1-mac3

4) Then I try ‘ping 10.60.101.109’ but I can’t.

From U-boot if I do 'ping 10.60.101.107', I get the following response:

      Using FM1@DTSEC3 device

      host 10.60.101.107 is alive

Note: I am not sure if I will get response when I will ping to t2080 u-boot from Linux host system.

 

Thanks and Regards,

Awadhesh Singh

 

 

0 件の賞賛
返信
1 解決策
2,332件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

U-Boot doesn't respond back to ARP(ping) requests.

So you cannot get responding from u-boot, when ping T2080RDB from Linux host PC.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,333件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

U-Boot doesn't respond back to ARP(ping) requests.

So you cannot get responding from u-boot, when ping T2080RDB from Linux host PC.

0 件の賞賛
返信