Hello,
I am not able to get uboot console on ls1012a freedom board.
Initially on this board RCW file was flashed using codewarrior tap . After than this board did not come up with u-boot console.
After that I setup yocto on ubuntu (14.04) host system and build binaries using bitbake fsl-image-full command. And flashed PBL file(0x0 offset) and u-boot (0x100000 offset) using codewarrior tap . But result is same. device did not come up with u-boot prompt.
Can anyone help to resolve this issue? Please let me know if I am missing anything.
Regards,
Kishan Patel
Solved! Go to Solution.
If you built RCW and u-Boot with bitbake, make sure you byte-swapped them before programming. Alternatively, use the most recent SDK pre-built u-Boot and RCW. Visit the link below to download SDK pre-built binaries:
Other recommendations for u-Boot/RCW deployment and board recovery can be found at the links below:
Have a great day,
Platon
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
I have gone through it. I am using SDK-V2.0-1703. There is no change in behavior after flashing prebuilt image.
I have used following command to flash binaries.
fl_write 0x0 PBL_0x33_0x05_800_250_1000_default.bin
fl_write 0x100000 u-boot-qspi-2016.09+fslgit-r0.bin
and reset board. But did not get any u-boot console.
After that i tried to full flash-image provided with SDK and write it from 0x0 location.
fl_write 0x0 QorIQ_SDK_V2.0_LS1012AFRDM_20170331_QSPI_Flash.bin
the result is same. did not get any u-boot console .
Regards,
Kishan Patel
If you built RCW and u-Boot with bitbake, make sure you byte-swapped them before programming. Alternatively, use the most recent SDK pre-built u-Boot and RCW. Visit the link below to download SDK pre-built binaries:
Other recommendations for u-Boot/RCW deployment and board recovery can be found at the links below:
Have a great day,
Platon
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
I also tried to swap bytes as you mentioned but did not work.
tclsh ./byte_swap.tcl u-boot-qspi-2016.09+fslgit-r0.bin swapped.bin 8
Regards,
Kishan Patel