UART Connections!

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

UART Connections!

1,093 次查看
qammarabbas
Contributor IV

Hi,

I am using UART of T1042. The device i am communicating with does not have the "CTS" and "RTS" pins as in UART of T1042. What should i do with the "UARTn_CTS_B" and "UARTn_RTS_B" pins of T1042? 

标记 (1)
0 项奖励
2 回复数

930 次查看
r8070z
NXP Employee
NXP Employee


Have a great day,

UARTn_RTS_B can be left unconnected. UARTn_CTS_ should be pulled up high through a2-10 kΩ resistor to DVDD (or else programmed as GPIO and output - see RCW[UART_BASE]).

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励

930 次查看
toddreed
Contributor I

Hi Serguei,

I see in AN4261 that the recommendation is to tie CTS high through a 2-10kΩ resistor to OVdd if CTS is not used.  We did not see this note and left UART_CTS0_B floating.  Is this an issue if we disable hardware flow control when turning on the port?  Is there any potential of damage, or is it just a floating input?

Thanks,

Todd

0 项奖励